LMFLASH like utility for Freescale Kinetis

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LMFLASH like utility for Freescale Kinetis

ソリューションへジャンプ
2,823件の閲覧回数
jparrish88
Contributor IV

Hello Freescale community.

I was hoping to find out whether or not anyone has seen a tool similar to this tool -

Stellaris® Flash Programmer, GUI and command line - LMFLASHPROGRAMMER - TI Software Fo…

for Freescale Kinetis parts.

The LMFLASH utility is a gui that performs flash read/writes over serial interfaces.

Most importantly, I was looking for ethernet.

Any help would be great.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,303件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Actual Kinetis devices can only be programmed through JTAG/SWD or eZPort.

For eZPort check AN4406. You could use Multilink from Pemicro and PROG for ARM (Pemicro as well)

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320138&CFID=470349&CFTOKEN=9938...

Then you can program bootloaders (USB, Serial, Ethernet,..) But first time programming of the bootloader has to be done using JTAG/SWD or eZPort.

Best Regards,

Luis

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,303件の閲覧回数
Monica
Senior Contributor III

Joshua, is this being useful?

Keep us posted! :smileyhappy:

0 件の賞賛
返信
2,303件の閲覧回数
deepakrana
NXP Employee
NXP Employee

hi

i guess you are looking for a standalone programmer. You can also check this link out :

Standalone Flash Programmer | MCU on Eclipse

Hope this helps

Cheers !!!!

2,304件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Actual Kinetis devices can only be programmed through JTAG/SWD or eZPort.

For eZPort check AN4406. You could use Multilink from Pemicro and PROG for ARM (Pemicro as well)

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320138&CFID=470349&CFTOKEN=9938...

Then you can program bootloaders (USB, Serial, Ethernet,..) But first time programming of the bootloader has to be done using JTAG/SWD or eZPort.

Best Regards,

Luis

0 件の賞賛
返信