LLWU using LPTMR0 on K22F not waking

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LLWU using LPTMR0 on K22F not waking

Jump to solution
1,148 Views
asfarley
Contributor IV

I'm trying to use the LLWU triggered by LPTMR0 on a K22F to wake from sleep. I've based my code so far on this guide:

Starting Point for Kinetis Low Power LLS Mode | MCU on Eclipse 

My goal is to put the system into low-power mode, then periodically wake using a low-power timer *without* resetting system state. So, I don't want to re-enter at main; I just want the MCU to pause while it's sleeping until the timer goes off.

The timer interrupt is being triggered but Cpu_OnLLSWakeUpINT is never executed after the processor goes back to sleep. Here's some background on my configuration:

-LPTMR0 configured to use LPO_1kHzSrc

-Very low power mode, Low leakage stop mode, Very low leakage stop mode all enabled under Cpu component

-LPTMR0 checked under "LLWU Settings" under Cpu component

-interrupt request enabled under LLWU Settings, Interrupts

-interrupt priority set to Highest

-Return to wait after ISR is disabled for both WAIT and SLEEP


My best guess is that this is happening because the TimerUnit_LDD interrupt handler is clearing the LPTMR0 before Cpu_OnLLSWakeUpINT gets executed. In fact, I can see this line in the PE-generated code for the timer unit:

PE_ISR(WakeupTimer_Interrupt)
{
/* {Default RTOS Adapter} ISR parameter is passed through the global variable */
WakeupTimer_TDeviceDataPtr DeviceDataPrv = INT_LPTMR0__DEFAULT_RTOS_ISRPARAM;

LPTMR_PDD_ClearInterruptFlag(LPTMR0_BASE_PTR); /* Clear interrupt flag */
WakeupTimer_OnCounterRestart(DeviceDataPrv->UserDataPtr); /* Invoke OnCounterRestart event */
}

What I don't understand: in the blog post above, the PE-generated code seems to be working fine according to the author.

Something I don't quite understand: what's the distinction between the TimerInterrupt event vs. the Cpu_OnLLSWakeUpINT event? If I have configured LPTMR0 as a LLWU source, I would expect that both the TimerInterrupt event and the LLSWakeUp event to occur. 

-------------------

Updates:

1) Could this be caused by the fact that LPTMR is enabled as an LLWU source but LPTMR_CMR is not? 

2) Somehow, *other* interrupts (not the LPTMR) are able to wake the processor and start it running again. I've set a breakpoint in Cpu_OnLLSWakeUpINT and it doesn't appear to be executed, so I'm not sure how or if the processor is waking. For example, I can transmit a UART character into my MCU (which triggers a different interrupt) and then everything starts running again. These other interrupts are not LLWU sources.

Labels (1)
0 Kudos
Reply
1 Solution
969 Views
asfarley
Contributor IV

Ok, I've got this partially solved: Cpu_OnLLSWakeUpINT is now being executed as intended.

I think the big change was using the mode DOM_STOP instead of DOM_WAIT. I never saw Cpu_OnLLSWakeUpINT execute after transitioning to DOM_WAIT. 

Under the Cpu component settings for PE, I noticed that the configuration under Low Power Mode Settings -> Operation Mode Settings -> WAIT does not have any drop-down box for selecting the equivalent ARM Cortex mode. This made me suspect that I was entering some unknown state using the function Cpu_SetOperationMode(DOM_WAIT, NULL, NULL).  

To answer some of my other questions in case someone else is reading: 

-I didn't have to modify any PE-generated code to get this working

-both Cpu_OnLLSWakeUpINT and the timer interrupt are being executed on wake despite the fact that both interrupts perform the following flag-clearing (this is the desired behavior from my perspective):

LPTMR_PDD_ClearInterruptFlag(LPTMR0_BASE_PTR); /* Clear interrupt flag */

The flag-clearing may be redundant and there may be other factors here, but at least future readers can confirm that waking from LLWU using LPTMR along with a TimerInt is possible (without reseting MCU either). 

View solution in original post

0 Kudos
Reply
1 Reply
970 Views
asfarley
Contributor IV

Ok, I've got this partially solved: Cpu_OnLLSWakeUpINT is now being executed as intended.

I think the big change was using the mode DOM_STOP instead of DOM_WAIT. I never saw Cpu_OnLLSWakeUpINT execute after transitioning to DOM_WAIT. 

Under the Cpu component settings for PE, I noticed that the configuration under Low Power Mode Settings -> Operation Mode Settings -> WAIT does not have any drop-down box for selecting the equivalent ARM Cortex mode. This made me suspect that I was entering some unknown state using the function Cpu_SetOperationMode(DOM_WAIT, NULL, NULL).  

To answer some of my other questions in case someone else is reading: 

-I didn't have to modify any PE-generated code to get this working

-both Cpu_OnLLSWakeUpINT and the timer interrupt are being executed on wake despite the fact that both interrupts perform the following flag-clearing (this is the desired behavior from my perspective):

LPTMR_PDD_ClearInterruptFlag(LPTMR0_BASE_PTR); /* Clear interrupt flag */

The flag-clearing may be redundant and there may be other factors here, but at least future readers can confirm that waking from LLWU using LPTMR along with a TimerInt is possible (without reseting MCU either). 

0 Kudos
Reply