LCDC Controller with DDR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCDC Controller with DDR

1,807件の閲覧回数
kaipaulus
Contributor III

I will to use the DMA to transfer data from DDR Controller directly to the LCDC Controller with the DMA engine. For the first calculation i need the Peak transfer rate for this transfer. In the user manual from K70 i find only the transfer rate for SRAM to Peripherial Device, not for Peripheral- to Peripheral-Device.

Is the DMA to be apple to solve this transfer? And what's about the max. Transfer Rate?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,622件の閲覧回数
apanecatl
Senior Contributor II

Hi Kai, the DMA can perform the transfer from the DDR controller to the LCDC, it counts as a 32b internal bus to internal SRAM memory transfer so you can use the following transfer rate table:

66.7 MHz, 32b          66.7

83.3 MHz, 32b          83.3

100.0 MHz, 32b      100.0

133.3 MHz, 32b      133.3

150.0 MHz, 32b      150.0


0 件の賞賛
返信

1,622件の閲覧回数
kaipaulus
Contributor III

Hi Pedro,

many thanks for the answer.

0 件の賞賛
返信