Hi @andy_kim
I hope you are doing well!
Both KL8x and K8x families do not have a dedicated LCD controller module, however they can drive LCDs using the Kinetis FlexIO peripheral.
The maximum resolution display, color depth and pixel clock frequencies should be estimated considering FlexIO module Bus bandwidth and the LCD setup. Please review the AN5280 Using Kinetis FlexIO to Drive a Graphical LCD section FlexIO_LCD Bus Bandwidth Performance to take a look at the technical details involved.
For example in the AN5280 The implementation of the TWRLCD-RGB module is demonstrated. This module includes a 480 x 272 graphical TFT LCD.
As you already may know the technical documentation of the KL81 and K81 MCUs is under NDA. If you would like, I can help you to get in contact with the appropriate team to help you to obtain documentation and review your project opportunity. We can check this by email.
If I can help you with other inquiries , please do not hesitate to let me know.
Diego