LCD type and Max LCD resolution that KL81 and K81 can support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LCD type and Max LCD resolution that KL81 and K81 can support

996 次查看
andy_kim
Contributor IV

Hello,

We're planning to mobile POS terminal with KL81 and K81 secure MCU.

We'd like to the LCD Type(RGB I/F or something else) and LCD Max resolution that KL81 and K81 can support.

 

Thanks,

Andy

0 项奖励
回复
1 回复

980 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @andy_kim 

I hope you are doing well!


Both KL8x and K8x families do not have a dedicated LCD controller module, however they can drive LCDs using the Kinetis FlexIO peripheral. 

The maximum resolution display, color depth and pixel clock frequencies should be estimated considering FlexIO module Bus bandwidth and the LCD setup.  Please review  the AN5280 Using Kinetis FlexIO to Drive a Graphical LCD section FlexIO_LCD Bus Bandwidth Performance  to take a look at the technical details involved.

For example in the AN5280  The implementation of the 
TWRLCD-RGB module  is demonstrated. This module includes a 480 x 272 graphical TFT LCD.

As you already may know the technical documentation of the KL81 and K81 MCUs is under NDA. If you would like, I can help you to get  in contact with the appropriate team to help you to obtain documentation and review your project opportunity. We can check this by email.

If I can help you with other inquiries , please do not hesitate to let me know.

Diego

0 项奖励
回复