KwikStik working with SD card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KwikStik working with SD card

2,122件の閲覧回数
gustavod
Contributor III

Hi,

 

For those who want to use a SD card with kwikStik we are pleased to announce our very first emulated SPI driver for SD card. We emulate the SPI pins trough IOs.

 

Now it is possible to access the SD card of the KwikStik kit. It is not so fast, but works.

 

Source code can be download here. We only tested it written into the FLASH (not in RAM).

http://brtos.googlecode.com/files/BRTOS%201.6x%20K40%20-%20SD%20card.rar

 

Regards,

Gustavo

0 件の賞賛
返信
1 返信

1,540件の閲覧回数
Dekiru
Contributor IV

Hi,

 

Kwikstik has test pads for SD card connector pins.

And unconnected SDHC0_D0~D3 are all connected to TWRPI or PCI connectors.

So I think we can enable SD card mode access by solder the test pads to that connector pins and set wrongly connected D4~D6 as input...

 

Regards

 

0 件の賞賛
返信