KwikStik SDHC issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KwikStik SDHC issue

1,918 次查看
gustavod
Contributor III

Hi everyone,

 

I'm trying to use a SD card on the kwikStik kit (K40x256).  I realized that SD card connector's data pins (DATA0~DATA3) are connected to SDHC0_D4~SDHC0_D7 while that pins are unused in 4 bits mode. So we cannot use SDHC support. So i tried to use the SD card trough SPI. However, SD card pin connections do not support SPI either.

 

This is really true? Freescale put a SD card slot connected to pins that we can not use?

 

0 项奖励
回复
1 回复

1,606 次查看
anthony_huereca
NXP Employee
NXP Employee

Unfortunately yes, you cannot use the SD Card slot in the current version of KwikStik's. It will be fixed on future versions.

 

See the KwikStik errata document here: http://cache.freescale.com/files/32bit/doc/errata/KWIKSTIKK40HWER.pdf

 

 

0 项奖励
回复