KwikStik SDHC issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KwikStik SDHC issue

1,890 Views
gustavod
Contributor III

Hi everyone,

 

I'm trying to use a SD card on the kwikStik kit (K40x256).  I realized that SD card connector's data pins (DATA0~DATA3) are connected to SDHC0_D4~SDHC0_D7 while that pins are unused in 4 bits mode. So we cannot use SDHC support. So i tried to use the SD card trough SPI. However, SD card pin connections do not support SPI either.

 

This is really true? Freescale put a SD card slot connected to pins that we can not use?

 

0 Kudos
Reply
1 Reply

1,578 Views
anthony_huereca
NXP Employee
NXP Employee

Unfortunately yes, you cannot use the SD Card slot in the current version of KwikStik's. It will be fixed on future versions.

 

See the KwikStik errata document here: http://cache.freescale.com/files/32bit/doc/errata/KWIKSTIKK40HWER.pdf

 

 

0 Kudos
Reply