Kl25z permanently secure (mass erase is disabled)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kl25z permanently secure (mass erase is disabled)

2,111 Views
Rafa_Mondragon
Contributor I
Is there a way in which I can unsecure the KL25z board? When I started the process of debugging, a message saying "Device is secure. Erase to unsecure?" appeared and I don't remember what did I clicked, but now when I try to debug it says "Permanently secure (mass erase is disabled). Try to unsecure anyways?", but despite clicking yes or no, the message keeps showing.
0 Kudos
Reply
4 Replies

2,100 Views
ErichStyger
Specialist I

If you did indeed secure your device (flash protection with mass erased), then you cannot unsecure it (as it would be against that concept).

See https://mcuoneclipse.com/2012/11/04/how-not-to-secure-my-microcontroller/ what securing means. Basically the debug probe tries to read from the device but fails and it returns the memory area as secured.

There is a small chance that it is a user error and your device is not secured (see https://mcuoneclipse.com/2012/05/28/device-is-secure/ ) so can you check that indeed you are using the correct device and connection.

Any indication what you did before? Indeed if you programmed a wrong binary with the wrong security bits, then your device is 'bricked' and you need to replace it.

I hope this helps,

Erich

 

0 Kudos
Reply

2,109 Views
Rafa_Mondragon
Contributor I

After clicking several times in the Try unsecure anyways, this window opens

Rafa_Mondragon_0-1617416183026.png

 

0 Kudos
Reply

1,980 Views
hfabbasi
Contributor III

@Rafa_Mondragon did you manage to find the solution? I am stuck with the same lock device problem and same message is being displayed once I try to flash the device. 

0 Kudos
Reply

2,110 Views
Rafa_Mondragon
Contributor I

permanently secure.PNG

0 Kudos
Reply