Kintesis QuadSPI Transmit Buffer does not transmits more 0x10 words to the attached N25Q256A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kintesis QuadSPI Transmit Buffer does not transmits more 0x10 words to the attached N25Q256A

ソリューションへジャンプ
1,953件の閲覧回数
bvsrkrishnarao
Contributor II

I am working on the TWR-POS-K81, with a on board N25q256A, when trying to program the NOR flash, QuadSPI block in the K82F doesn't transmit anything more than 0x10 words

the TBDR register seems to accepts only 0x10 words (64bytes) of data and freezes and loops waiting for QuadSPI_SR:TXFULL is always '1'to clear, The QuapSPI_BSR:TRCTR shows 0x20 and QuadSPI_TBSR:TRBFL - 0x10, the QuadSPI_SR:TXFULL is always '1'.

Trying to clear and check QuadSPI_FR:TBFF as per the document doesn't seem to help.

The LUT instruction programmed is

[16] = 0x08180432,  (0x32 is QUAD INPUT FAST PROGRAM)  I am running Extended-SPI mode

[17] = 0x22FF,

Any insights and help is most welcome

Thanks

Krishna

ラベル(2)
0 件の賞賛
返信
1 解決策
1,870件の閲覧回数
bvsrkrishnarao
Contributor II

I could solve the issue, by putting in some delay at each read of the QuadSPI_SR::TXFULL

Here is code snippet

while(QuadSPI_BRD_SR_TXFULL(base)){for (volatile uint32_t i=0; i < 100; i++) __ASM("nop");}

Earlier the driver would just loop if the TXFULL flag was set, while writing into TBDR register, just putting the delay seemed to have solved the issue.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,871件の閲覧回数
bvsrkrishnarao
Contributor II

I could solve the issue, by putting in some delay at each read of the QuadSPI_SR::TXFULL

Here is code snippet

while(QuadSPI_BRD_SR_TXFULL(base)){for (volatile uint32_t i=0; i < 100; i++) __ASM("nop");}

Earlier the driver would just loop if the TXFULL flag was set, while writing into TBDR register, just putting the delay seemed to have solved the issue.

0 件の賞賛
返信
1,870件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Krishna,

Thank you for the share info.

Hope your answer could help other customers.

best regards,

Ma Hui

0 件の賞賛
返信