Kinetis micro controller internal flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis micro controller internal flash

1,497 次查看
dotangoldberg
Contributor II

Hello,

I'm trying to build infrastructure for write/read small size data (around 1~2 KB) into the internal flash using FRDM-K64F.

The write/read designated flash sectors must not be over written upon the OS & application binary flashing

1. Is there a PC tool that can support flashing specific flash sectors? (for example not flashing the last xx sectors)?

2. Is it possible to manage the internal flash (or part of it - for example the write/read area) as a file system?

Thanks a lot,

Dotan

0 项奖励
回复
1 回复

1,399 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi dotan goldberg 

If you are using P&Emicro interface to flash your device, you can used the advanced option. it gives you the ability to preserve FLASH ranges.

Please check the following post as reference.

https://mcuoneclipse.com/2015/04/16/updated-pe-gdb-server-for-eclipse-connectattach-and-advanced-fla... 

Hope this information help you.
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复