Kinetis family library device file - documentation/appnote

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis family library device file - documentation/appnote

1,009 次查看
tylernguyen
Contributor I

Hi,

Does anybody know of any documentation or application notes describing meaning/functionality of the thousands of registers defined in the device library files? for the Kinetis family devices ie MK20F12.h and such  ....

Thanks

0 项奖励
回复
2 回复数

903 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello tylernguyen:

What do you mean with device library files? Are you referring to Kinetis header files (e.g. the MK20F12.h)?

For each Kinetis device there are two main documents:

Datasheet: Contains general technical information/specs.

Reference Manual: Describes the registers, memory, peripherals and all the info you need.

So the one you may be looking for is the Reference Manual. This can be found in the "Documentation" tab of the specific product page. For example for K20_120 MHz parts the page is in the next link:

K20_100 |Kinetis 20 100 MHz MCUs|Freescale

You will find several manuals, datasheets and application notes. The Reference Manuals and datasheets are divided by package (81 pin, 100 pin, etc). Just choose the ones for your part.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

903 次查看
mjbcswitzerland
Specialist V

Hi

They are all described in the user manuals. For the K20F120 see http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=K20_120&fpsp=1&tab=Documentation_Tab

Specifically http://cache.freescale.com/files/microcontrollers/doc/ref_manual/K20P144M120SF3RM.pdf?fasp=1&WT_TYPE...

Regards

Mark

Kinetis: µTasker Kinetis support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 项奖励
回复