Kinetis X - Will it happen?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis X - Will it happen?

ソリューションへジャンプ
2,863件の閲覧回数
markoseverin
Contributor II

Hi guys,

Some documents on the freescale website (like http://www.freescale.com/files/32bit/doc/fact_sheet/KINETISXSERIESFS.pdf), mention the X series of Kinetis. The press release was made at the end of 2011, but till now there has not been any news on the X family. Is the X familly still planned to be released, or was this plan abandoned?

Thanks and best regards,

Merko

タグ(2)
1 解決策
2,175件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Marko

Up to now, I never heard X series product plan is stop from my side. So I think it should be in progress.

Hope my reply can help you.

Best Regards

Paul

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,175件の閲覧回数
pupospace
Contributor I

I am also interested in the series x, the link that is located in PDF has been removed

http://freescale.com/Kinetis/xseries

I think that the project has been abandoned, there is no information of presample or more info

0 件の賞賛
返信
2,176件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Marko

Up to now, I never heard X series product plan is stop from my side. So I think it should be in progress.

Hope my reply can help you.

Best Regards

Paul

0 件の賞賛
返信