Kinetis SPI code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis SPI code

Jump to solution
5,407 Views
RonBurgundy
Contributor I

Hello,

Does anyone have or know where I can get some sample SPI code for the K40 chip?  I downloaded the KINETIS512_SC file from Freescale and it seems like they have sample code for everything except SPI.

 

Thanks.

0 Kudos
Reply
1 Solution
3,895 Views
freegeek
Contributor III

Download CW10 and create simple project using Processor Expert to create a SPI driver and the look at the PE code.

View solution in original post

0 Kudos
Reply
2 Replies
3,896 Views
freegeek
Contributor III

Download CW10 and create simple project using Processor Expert to create a SPI driver and the look at the PE code.

0 Kudos
Reply
3,895 Views
mnorman
NXP Employee
NXP Employee

Processor Expert in CodeWarrior 10.1 is quite advanced for the 32-bit MCUs.  There are physical device drivers and logical device drivers available that provide rich APIs.  Check it out!

 

-mnorman