Kinetis SPI code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,397件の閲覧回数
RonBurgundy
Contributor I

Hello,

Does anyone have or know where I can get some sample SPI code for the K40 chip?  I downloaded the KINETIS512_SC file from Freescale and it seems like they have sample code for everything except SPI.

 

Thanks.

0 件の賞賛
返信
1 解決策
3,885件の閲覧回数
freegeek
Contributor III

Download CW10 and create simple project using Processor Expert to create a SPI driver and the look at the PE code.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,886件の閲覧回数
freegeek
Contributor III

Download CW10 and create simple project using Processor Expert to create a SPI driver and the look at the PE code.

0 件の賞賛
返信
3,885件の閲覧回数
mnorman
NXP Employee
NXP Employee

Processor Expert in CodeWarrior 10.1 is quite advanced for the 32-bit MCUs.  There are physical device drivers and logical device drivers available that provide rich APIs.  Check it out!

 

-mnorman