Kinetis SDK FLASH_ProgramPartition() from fsl_flash.c example code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis SDK FLASH_ProgramPartition() from fsl_flash.c example code

1,424 次查看
phil74
NXP Employee
NXP Employee

Hello,

 

Do we have any example code to setup the EEPROM on MK10DX128 (or K60) with SDK2.2  and especially how to use "FLASH_ProgramPartition" from fsl_flash.c ?

 

Thanks in advance,

Best Regards,
Philippe.

标签 (1)
0 项奖励
回复
1 回复

1,331 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Philippe.

I would suggest you refer to AN4282, Using the Kinetis Family Enhanced EEPROM Functionality

https://www.nxp.com/docs/en/application-note/AN4282.pdf 


and check the section 3.1 FlexMemory partitioning.

If you want to repartition the EEPROM, it is said  you can mass erase the chip FlexNVM, and do the EEPROM partitioning.

Regards

Daniel

0 项奖励
回复