Kinetis Motor Suite can't connect the mcu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Motor Suite can't connect the mcu

1,901 Views
zhigangpi
Contributor I

Hi guys, I'm working with KMS with HVP-KV31F120M.After I started a new KMS project-HVPKV31F120M_SNLESSVEL_IAR_1_0_0_1, KMS cannot connect my mcu, my development platform is HVP-MC3PH,my Control board is HVP-KV31F120M.

搜狗截图20160331220528.png

There are the versions of softwares in my pc:

KMS1.0.0,

Microsoft® .NET Framework 4.6,KSDK1.3.0,

IAR Embedded Workbench for ARM® 7.40,

openSDA USB Driver Version 12.3,

the Application Version of the Mass Storage/Debug App of HVP-KV31F120M is 1.18.

搜狗截图20160401203027.png

Then I load .OUT file and download the image to the MCU following the KMS100UG.pdf, and retry communication via the Configure Communication Port option,communication still failed.This problem also exists in TWRKV31F120M. why and what should I do?

图片1.png

搜狗截图20160401203224.png

Thanks and regards.

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,561 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, ZhiGang,

现在, 你能连上板子吗? 如果不能,方便留个电话吗?

BR

XiangJun Rong

0 Kudos
Reply

1,561 Views
zhigangpi
Contributor I

抱歉回复晚了,感谢您的回复,现在KMS还是连不上HVPKV31板子,但是FRDM-KV31F可以连上,是不是只有标了ENABLED BY KMS的板子才能用KMS呢,我的电话是(86)13430370664.

0 Kudos
Reply