Hi all,
I have a question.
In the Reference manual IIC chapter : The interface is designed to operate up to 100 kbit/s with maximum bus loading and timing.
Does the Kinetis MCU support IIC in the fast mode ?
Thanks!!
已解决! 转到解答。
 
					
				
		
 carlos_neri
		
			carlos_neri
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		As Jim commented, 100Kbps is the maximum data rate when the bus is at its maximum capacitance load (400pF). If you do not have that amount of capacitance load, the I2C can achieve fast mode (400kbps).
 
					
				
		
 carlos_neri
		
			carlos_neri
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		As Jim commented, 100Kbps is the maximum data rate when the bus is at its maximum capacitance load (400pF). If you do not have that amount of capacitance load, the I2C can achieve fast mode (400kbps).
Have a look at the I²C specification and manual of NXP:
http://www.nxp.com/documents/user_manual/UM10204.pdf
On page 55 there are easy formulas & charts to determine pull-up values to meet the rise time requirements. Alternatively, take a look at the timing specs themselves in chapter 6.
On other Freescale chips, under ideal conditions I have run I2C at 1.2Mhz just as a test (I have not had a chance to test this one yet).
Note that this is really an overall specification of the I2C bus, not so much the part itself. Also a lower pull up helps for faster speeds.