Kinetis L ADC Offset Correction

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis L ADC Offset Correction

ソリューションへジャンプ
2,464件の閲覧回数
wendersonolivei
Contributor IV

Hi all,

I'm trying to acquire the value of many ADC inputs on my FRDM-KL25Z. Actually, I saw the example Measuring all ADC inputs on FRDM-KL25 using DMA and i'm trying to do this. But, I don't understand very well the ADC Offset Correction Register.

In this example, that register is set to 4U. I just don't understand why. Can someone explain that?

Thank you!

ラベル(2)
タグ(3)
1 解決策
1,981件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi,Oliverira

This register is used to correct ADC calibration. For example, you calibration our ADC module by a external standard power supply. Then you can transfer data to register ADCx_OFS after you compare testing result and expected result.

Best Regards

Paul

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,982件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi,Oliverira

This register is used to correct ADC calibration. For example, you calibration our ADC module by a external standard power supply. Then you can transfer data to register ADCx_OFS after you compare testing result and expected result.

Best Regards

Paul

0 件の賞賛
返信