Kinetis Kl17 uart iso7816

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis Kl17 uart iso7816

2,658 次查看
HeMyFAE
NXP Employee
NXP Employee

Dear Kinetis SDK.

I downloaded the latest sdk for Kinetis KL17 / KL43  looking for driver support for iso 7816 for UART.

I scan the skd api rm but couldn't find any reference for 7816 api driver code support.

Questions:

1) Is there a separate driver that I can download to integrate into the KL17 to support 7816?

2) is there any appnote for the 7816 driver code?

3) Any specific instruction on HW design/set up to support 7816 interface?

Regards,

hy

标签 (1)
0 项奖励
回复
2 回复数

2,417 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Hy Mai,

    After I receive your email, I also checked the related code, but about the KL series smart code, I just find the AN5218, no related code.

   But I find our K series, there are some SDK code about the ISO7816 smart code.

  \SDK_2.3.1_TWR-K21F120M\boards\twrk21f120m\demo_apps\emvl1

The related driver can be found in folder:

SDK_2.3.1_TWR-K21F120M\devices\MK21FA12\drivers

BTW, this post may also useful to you:

Smart Card APIs for K2x 

I think you can let our refer to the K series smart code at first.

 About the Chinese application note related code, I will try to contact with the author, but I am not sure he still in NXP or not.

Any updated information, I will let you know.

Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

2,417 次查看
HeMyFAE
NXP Employee
NXP Employee

customer : Sierra wireless

0 项奖励
回复