Kinetis KL03 - Program retention after power cycle

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Kinetis KL03 - Program retention after power cycle

跳至解决方案
2,413 次查看
armaram
Contributor III

Hi,

My #kl03 doesn't retain program after power cycle. We must reprogram the MCU in order to continue working. We are using the PE Micro Multilink FX cable to program the MCU.

Can anyone pls help?

Thanks,

Arvind

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
2,135 次查看
gnichimohamed
Contributor III

Check if nmi_b pin is low or pulled down low then you need to disable nmi.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,135 次查看
miduo
NXP Employee
NXP Employee

Hi,

Please let me know what board you used and what software used? I mean the flash programming method. What steps you had done and if any error reported?

0 项奖励
回复
2,135 次查看
armaram
Contributor III

It's a custom hardware board. We use

-KSDK1.3.1.

-Programming cable - PEMicro multilink fx

-SWD port

Pls let me know if you need any further information.

No errors reported. Only that we have to reprogram the MCU everytime we do a power cycle. We want the program to be retained even when power is turned OFF/ON.

0 项奖励
回复
2,136 次查看
gnichimohamed
Contributor III

Check if nmi_b pin is low or pulled down low then you need to disable nmi.

0 项奖励
回复
2,135 次查看
armaram
Contributor III

Yes, in fact that was the problem. One of the NXP guys helped us out but I missed to post the update. Thank you though!

0 项奖励
回复
2,135 次查看
armaram
Contributor III

@Fang Li any help would be great! 

0 项奖励
回复