Kinetis KL03 - Program retention after power cycle

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis KL03 - Program retention after power cycle

ソリューションへジャンプ
2,335件の閲覧回数
armaram
Contributor III

Hi,

My #kl03 doesn't retain program after power cycle. We must reprogram the MCU in order to continue working. We are using the PE Micro Multilink FX cable to program the MCU.

Can anyone pls help?

Thanks,

Arvind

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,057件の閲覧回数
gnichimohamed
Contributor III

Check if nmi_b pin is low or pulled down low then you need to disable nmi.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,057件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Please let me know what board you used and what software used? I mean the flash programming method. What steps you had done and if any error reported?

0 件の賞賛
返信
2,057件の閲覧回数
armaram
Contributor III

It's a custom hardware board. We use

-KSDK1.3.1.

-Programming cable - PEMicro multilink fx

-SWD port

Pls let me know if you need any further information.

No errors reported. Only that we have to reprogram the MCU everytime we do a power cycle. We want the program to be retained even when power is turned OFF/ON.

0 件の賞賛
返信
2,058件の閲覧回数
gnichimohamed
Contributor III

Check if nmi_b pin is low or pulled down low then you need to disable nmi.

0 件の賞賛
返信
2,057件の閲覧回数
armaram
Contributor III

Yes, in fact that was the problem. One of the NXP guys helped us out but I missed to post the update. Thank you though!

0 件の賞賛
返信
2,057件の閲覧回数
armaram
Contributor III

@Fang Li any help would be great! 

0 件の賞賛
返信