Kinetis K82 Debug Port - Enabling SWD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Kinetis K82 Debug Port - Enabling SWD

跳至解决方案
2,348 次查看
greycon
Contributor II

I see from the K82 Ref Manual that the Debug Port comes up as JTAG after reset. But I am working with a FRDM-K82F eval board, for early prototyping, and it is set to SWD. But I can't find where in any of the code the K82 Debug Port is changed from JTAG to SWD.

Can you tell me how this is done? As I will ultimately need to do this on our future board.

标签 (1)
0 项奖励
回复
1 解答
2,343 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi greycon,

Please refer "11.4.1 JTAG-to-SWD change sequence" of Kinetis K82: 150MHz Cortex®-M4F up to 256KB Flash (144pin)

11.4.1 JTAG-to-SWD change sequence.png

OpenSDA(debugger) has done this.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,344 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi greycon,

Please refer "11.4.1 JTAG-to-SWD change sequence" of Kinetis K82: 150MHz Cortex®-M4F up to 256KB Flash (144pin)

11.4.1 JTAG-to-SWD change sequence.png

OpenSDA(debugger) has done this.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
2,340 次查看
greycon
Contributor II

Ah, openSDA - of course! Many thanks for your reply Robin.

Cheers,

Con

0 项奖励
回复