Kinetis K8 FlexIo max serial clock speed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis K8 FlexIo max serial clock speed

4,206 次查看
AlainRIMLINGER
Contributor I

Hello. I would like to connect K8x Kinetis secure licrocontroller with SPI at higher rate than 24MHz. Can I use FlexIo interface to achieve this ? What would be the max speed of the FlexIO interface serial clock ? Thank you very much. Regards

标签 (1)
0 项奖励
回复
2 回复数

3,682 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Alain RIMLINGER,

     From the K8X datasheet, you may know, the SPI operation frequent is 30Mhz, I don't know what the SPI frequent you want to achieve.

    If you want to use the FlexIO,  the clock speed may be higher, because the  FlexIO clock can up to 150Mhz.

    More detials about the FlexIO, please refer to this post:

Understanding FlexIO

Wish it helps you!

If you still have question, please contact with me!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,681 次查看
AlainRIMLINGER
Contributor I

Hello

Thank you very much.

It will help win the socket for NXP.

With best regards, Alain

Alain Rimlinger

Field Application Engineer

Arrow Electronics

13-15 rue du Pont des Halles

94656 Rungis Cedex

T +33 1 49 78 49 25

M +33 6 86 53 35 52

[email protected]<mailto:[email protected]>

www.arrow.com<http://www.arrow.com/>;

De : kerryzhou

Envoyé : mardi 16 février 2016 06:10

À : Alain Rimlinger

Objet : Re: - Kinetis K8 FlexIo max serial clock speed

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Kinetis K8 FlexIo max serial clock speed

reply from Jingjing Zhou<https://community.freescale.com/people/kerryzhou?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion<https://community.freescale.com/message/614738?et=watches.email.thread#614738>

0 项奖励
回复