Kinetis K66 flashing issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K66 flashing issue

1,164 Views
anand_s
Contributor III

Hi all,

        We are using  K66 controller in our board. Codewarrior 11.1 is the IDE and MQX 4.2.0 is the RTOS. The application program can successfully debug and its working fine in 'Int Flash Debug' mode. Now for testing purpose we are using default linker(In the BSP directory) .Then we generated .hex file (srec) of the same and tried to flash it, Flashing is successfully happened but code is not executing.Then i tried  'Int Flash Release', then also same problem happened.  For flashing the .hex file i am using P&E Multilink.  So what is i am missing here? I can successfully flash the code but why its not executing? Please help me out..

Thanks and regards, 

 Anand.S

0 Kudos
Reply
1 Reply

1,115 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

I test on my TWR-k65 board. It seems fine. Which MQX example do you use? And how you generate hex file and download?

Regards,

Jing

0 Kudos
Reply