Kinetis K40x256 Tower with TWR-SER Ethernet Example?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis K40x256 Tower with TWR-SER Ethernet Example?

2,718件の閲覧回数
thales_user1
Contributor I

Hi there,

 

Note: I accidentally posted this message in the wrong forum, so if you have already seen it apologies.

 

We have just purchased a couple of Kinetis K40x256 Tower evaluation boards. We are using the IAR v6.21 IDE to build and load the software to the board. We are able to use the TWR-K40X256_Quick_Start_Demo, however we cannot find any help or documentation on how to interface with the TWR-SER peripheral board, specifically how to drive the Ethernet port.

 

What we are really looking for is an example and/or instructions on how to drive the Ethernet port on the TWR-SER via the tower bus interface from the TWR-K40x256. Failing that we would appreciate a point in the direction of some documentation.

 

The closest things we have found are the 4-page leaflet in the TWR-SER box which describes the jumpers we need to set for Ethernet usage and the K40 tower user manual, which is similarly quite light on information.

 

Any help, greatly appreciated.

 

Best regards

thales_user1

0 件の賞賛
返信
3 返答(返信)

2,143件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

The K40 doesn't have an Ethernet controller and so it can't be used with the Ethernet port on the TWR-SER board.

 

To use Ethernet you need the TWR-K60N512 processor board.

 

Regards

 

Mark

 

0 件の賞賛
返信

2,143件の閲覧回数
Ruds
Contributor I

I am using K60N512 , and downloaded TWR-K60N512 processor board programs, but i din't find ETHERNET application on that.

is there any application code on Ethernet?

0 件の賞賛
返信

2,143件の閲覧回数
emh203
Contributor II

For bare Metal Examples get the "Kinetis_SC" sample code

 

If you are interested in an RTOS,  MQX has a bunch of ethernet application examples for the K60 board.

0 件の賞賛
返信