Kinetis K40 using GPIO as supply and current capability

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis K40 using GPIO as supply and current capability

ソリューションへジャンプ
2,303件の閲覧回数
lucianomoraes
Contributor I

Hi, I want to use a GPIO of the Kinetis K40 as specific supply for other ic but I didn't find a list of the GPIOs that can be used as supply (all GPIOs can be used as supply pins or only some GPIOs have a internal charge pump for it?) and the specification of the GPIO pin on supply mode mainly current capability and voltage range operation in the referece manual. Someone can point me where can I find this info?

Thanks,

Luciano.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,962件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

K40 GPIO pins provide two drive strength: high drive strength and low drive strength.

Please check below table to find the drive strength capability:

GPIO Drive.png

The GPIO pin could provide drive current about 9mA.

If customer want to use GPIO pin to drive as power supply, I don't think GPIO pin could provide enough drive current.

The K40 provides USB voltage regulator, which could output 3.3V with Max. 120mA drive current at VOUT33 pin.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,963件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

K40 GPIO pins provide two drive strength: high drive strength and low drive strength.

Please check below table to find the drive strength capability:

GPIO Drive.png

The GPIO pin could provide drive current about 9mA.

If customer want to use GPIO pin to drive as power supply, I don't think GPIO pin could provide enough drive current.

The K40 provides USB voltage regulator, which could output 3.3V with Max. 120mA drive current at VOUT33 pin.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,962件の閲覧回数
lucianomoraes
Contributor I

Thanks, your help, Hui_Ma and Jorge_Gonza!

0 件の賞賛
返信