Kinetis K24 example projects in IAR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis K24 example projects in IAR

2,510 次查看
annamol
Contributor IV

Hi,

Is there example projects for K24 in IAR? If yes, it would be great if someone can share the download link..

I have been searching for that for quite some time.

标签 (1)
0 项奖励
回复
3 回复数

1,917 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Annamol Alex,

If you installed KSDK 1.2, you may find demos for TWR-K24F120M in the folder of "C:\Freescale\KSDK_1.2.0\examples\twrk24f120m", which supports multiple IDEs including IAR. To download KSDK 1.2, please refer to Software Development Kit for Kinetis MCUs|Freescale

Hope that helps,


Have a great day,
Kan

Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,918 次查看
annamol
Contributor IV

Hi kan,

I am new to Kinetis SDK environment. I have been working with bare metal coding and MQX coding for K53 for the last few months in IAR. So I am just curious regarding KSDK and the advantages it has over bare metal in terms of power consumption? This is because we shifted from MQX to bare metal because of power constraints for an application.

So please do suggest which will be the better way to go about for K24 in terms of coding and support.

1) Bare metal

2) MQX

3) KSDK

And one more doubt, isn't there example projects in IAR just like the ones K53 had(KINETIS_v2_SC.zip)? Can bare metal approach be used for K24 ?

0 项奖励
回复

1,918 次查看
mjbcswitzerland
Specialist V

Hi

You can get the quick start package for the TWR-K24F120M from

TWR-K24F120M Quick Start Package

Usually they include IAR examples.

There is also a complete solution for the K24 and IAR at the links below.

Regards

Mark

Kinetis: µTasker Kinetis support

K24: µTasker Kinetis TWR-K24F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 项奖励
回复