Kinetis K22 TWR-K22F120M + TWR-SER2 USB High-Speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K22 TWR-K22F120M + TWR-SER2 USB High-Speed

Jump to solution
1,587 Views
nbgatgi
Contributor IV

Does the enhanced serial tower board (TWR-SER2) make high-speed (HS) USB possible with the Kinetis K22 tower board (TWR-K22F120M)?

0 Kudos
Reply
1 Solution
1,472 Views
mjbcswitzerland
Specialist V

Hi Nick

The K22 doesn't have a HS USB controller (just full-speed) and so can't be used with the HS USB transceiver on the SER2 board.

Regards

Mark

http://www.utasker.com/services.html

View solution in original post

1 Reply
1,473 Views
mjbcswitzerland
Specialist V

Hi Nick

The K22 doesn't have a HS USB controller (just full-speed) and so can't be used with the HS USB transceiver on the SER2 board.

Regards

Mark

http://www.utasker.com/services.html