Kinetis K21

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K21

Jump to solution
3,280 Views
pushpraj
Contributor I

Which are the DAC pin in MK21FN1M0AVLQ12 (LQFP 144) ????

I cant find it in datasheet pinout page???

0 Kudos
Reply
1 Solution
3,271 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Yes. The LQFP doesn't have the DAC pin. LQFP can't use the dac.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
3,269 Views
KalaimaniArumugam
Contributor III

Thank you for this reply, I am also facing same problem in my design. But i refer  "Kinetis K Series Microcontrollers (MCUs)
Selector Guide.pdf" for controller selection, it mentioned that MK21FN1M0AVLQ12 support two DAC(find the attachment). If it's correct please update the document.

KalaimaniArumugam_0-1628580040474.jpeg

 

0 Kudos
Reply
3,264 Views
nxf56274
NXP Employee
NXP Employee

Hi,

The RM and datasheet are more correct. The selector has some mistakes.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,256 Views
pushpraj
Contributor I

Thank you for the answer.

I was also confused because of selector guide.

0 Kudos
Reply
3,272 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Yes. The LQFP doesn't have the DAC pin. LQFP can't use the dac.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply