Kinetis K10 datasheet discrepancy - MCG_C1 --> IREFS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis K10 datasheet discrepancy - MCG_C1 --> IREFS

1,427 次查看
ignisuti
Contributor IV

I'm curious if there is a discrepancy on page 528 of the Manual. 


It says that IREFS value for MCG_C1 selects either the External Reference Clock or the slow internal reference clock.

But, if MCG_C2 --> IRCS is configured to use the Fast internal reference clock, then IREFS would be fast, not slow... right?

0 项奖励
回复
2 回复数

1,184 次查看
apanecatl
Senior Contributor II

To use the Fast internal reference clock you only need to set IRCS as Fast Internal Reference Clock enabled (1), the state of IREFS is irrelevant once you set IRCS

0 项奖励
回复

1,184 次查看
kidfy
Contributor I

yes, but before you select the fast clock mode, you need check the FRDIV ,and make sure the clock source for FLL is between 31.25khz-39.025khz.

0 项奖励
回复