Kinetis K10 datasheet discrepancy - MCG_C1 --> IREFS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K10 datasheet discrepancy - MCG_C1 --> IREFS

1,431 Views
ignisuti
Contributor IV

I'm curious if there is a discrepancy on page 528 of the Manual. 


It says that IREFS value for MCG_C1 selects either the External Reference Clock or the slow internal reference clock.

But, if MCG_C2 --> IRCS is configured to use the Fast internal reference clock, then IREFS would be fast, not slow... right?

0 Kudos
Reply
2 Replies

1,188 Views
apanecatl
Senior Contributor II

To use the Fast internal reference clock you only need to set IRCS as Fast Internal Reference Clock enabled (1), the state of IREFS is irrelevant once you set IRCS

0 Kudos
Reply

1,188 Views
kidfy
Contributor I

yes, but before you select the fast clock mode, you need check the FRDIV ,and make sure the clock source for FLL is between 31.25khz-39.025khz.

0 Kudos
Reply