Kinetis K USB CDC makefile project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis K USB CDC makefile project

1,461件の閲覧回数
pkaar
Contributor I

I am looking for an example/tutorial for USB CDC on Kinetis K devices. I want to avoid Processor Expert or KDS examples. Best would be a step-by-step instruction how to get USB CDC working without using any tools. What files need to be copied, what files need to be adjusted?

Best regards,

Philipp

0 件の賞賛
返信
1 返信

1,298件の閲覧回数
mjbcswitzerland
Specialist V

Hi

You can get out-of-the-box makefile based USB-CDC in the uTasker project:

- http://www.utasker.com/docs/uTasker/USB_User_Guide.PDF

- http://www.utasker.com/docs/uTasker/uTaskerV1.3_USB_Demo.PDF

It allows multiple USB-CDC interfaces for communication (including MODBUS) or USB-UART bridging with complete end-to-end flow control (see reference with 6 USB-CDC-UART bridges at http://www.utasker.com/kinetis/TWR-K64F120M.html).

The USB-CDC supports also RNDIS (for virtual Ethernet) and can be combined with MSD, Audio, HID without any effort - see http://www.utasker.com/kinetis/USB_Device.html

Industrially proven in many Coldfire products since 2008, and Kinetis K and KLs from 2011 - including unique USB simulation to simplify/accelerate application level development and testing as well as software auditing.

Not based on PE or KDS examples and requires no tools. Small memory footprint, extensively tested and maintained for professional requirements. One-on-one email/tel. support where required.

Freely available as open-source at http://www.utasker.com/forum/index.php?topic=1721.0 in case no support is desired (some newest features may be missing in anonymous download versions).

Regards

Mark

0 件の賞賛
返信