Kinetis IPV6 availability

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis IPV6 availability

3,012 次查看
kfranz
Contributor III

What options do I have for IPV6 on the Kinetis K60?

0 项奖励
回复
4 回复数

2,322 次查看
admin
Specialist II

If by Kinetis K60 you are referring to the K60 Tower kit, then you can use the lwip port that Freescale provides in their example projects download. Although the demo is set to use IPv4, lwip supports IPv6.

0 项奖励
回复

2,322 次查看
kfranz
Contributor III

Thank you for the information. We have the K60 tower from a seminar a few months ago. Haven't opened it yet. We plan to open it up and start some serious evaluation in the next few weeks. One of the requirements is IPV6.

 

http://lwip.wikia.com/wiki/IPv6 says, "The code for IPv6 in lwIP is highly experimental and has not been maintained." . That makes me a little nervous. Does anyone kknow if this is still true? lwip is a dual stack, IPv4/IPv6 implementation which I like.

 

Do you or anyone out there have any experience with IPv6? I don't even know what questions to ask regarding IPv6. For example, what protocols must change to work with IPv6?

 

thanks,

Kevin

0 项奖励
回复

2,322 次查看
PaoloRenzo
Contributor V

Hi Kevin

 

Did you get any luck with IPv6? Would like to try lwIP, but maybe you have more news on this regard

 

Thanks!

0 项奖励
回复

2,322 次查看
butok
NXP Employee
NXP Employee

Hi Guys,

 

Just for FYI:

Now we are working on adding of IPv6 to RTCS. It will be dual IPv4/IPv6 stack (you will be able to enable both or only one).

First version of RTCS-IPv6 should be available in the next major release of MQX.

It should pass (or is already passing :smileywink: ) the “Silver IPv6 core certification” tests.

The first version supports/tested with Ethernet interface only (TBD later PPP or WiFi).

 

Also I am working on adding of IPv6 to FNET (bare-metal TCP/IP stack).

As RTCS IPv6 and FNET IPv6 are developed by the same guy, the core IPv6 logic of  RTCS and FNET will be very close => more easier to support/fixing.

 

BTW:

Please do not ask about concrete dates and sending early releases.

It should be available during this year.

 

Thanks,

Andrey Butok

0 项奖励
回复