Kinetis IO mux for Analog pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis IO mux for Analog pin

1,780 次查看
daweiyou
NXP Employee
NXP Employee

Hi guys:

I have a question about analog pin, for example ADC0_SE pin, the default mux is ADC pin, and could change to GPIO output functionality after reset.

But before the GPIO output take effect, what's the output? Hi-Z or undifined?

标签 (1)
2 回复数

1,324 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Dawei:

For digital-only pins, the default is Disabled (High Impedance). But for default analog pins, it depends on the internal circuitry. In this case for ADC, there is not an output, and the voltage level depends on your external circuitry. Give a check to the next diagram about internal circuitry for ADC pins:

ADC_pin.png

Hope this helps.

Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,323 次查看
daweiyou
NXP Employee
NXP Employee

Hi Jorge:

thx your reply.

the input pin, marked yellow, is other ADC input channel.

And from above simplified input circuit, the ADC pin, as ouput maybe undefined level, the Radin and Cadin determine Zadin, which is not large.

0 项奖励
回复