Kinetis I2C ODE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis I2C ODE

2,384件の閲覧回数
dieterteuchert
Contributor IV

Yesterday i implemented a test setup with a PCM1690 audio DAC, using KL10 I2C1 for control. When i looked at SDA with the scope, i found the ACK from the slave was at about 0.4 V. Though within specs, this looked ugly. I checked the pullup current and found the pullup resistor was about 150 Ohm. The error was in the I2C1 pin configuration. When i used the PORTx_PCRn configuration bit ODE (open drain enable) in addition to the pin MUX setting, everything looked perfect.

I am writing this note, because it's an error that may go unnoticed. I don't have time to check the Kinetis sample code, today i have to do the I2S part.

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,885件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Dieter

I think you use K10 not KL10. If you use K series, you need to enable ODE bit when you use I2C module. Then you make these pins to be a open drain pin.

Hope my reply can help you.

Best Regards

Paul

0 件の賞賛
返信

1,885件の閲覧回数
dieterteuchert
Contributor IV

I did not want to start a discussion, but sorry, your reply was useless.

I reported unexpected behaviour when using I2C with a Kinetis processor (Totem-Pole SDA). It is not a problem nor an issue, just unexpected behaviour. While you may have been aware of this, you did not give any useful information which parts are affected. I think, my recommendation to use the ODE bit was valid and useful.

0 件の賞賛
返信