Kinetis FlexNVM partition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis FlexNVM partition

1,655件の閲覧回数
LPs
Contributor III

Hi all,

I'm trying to understand how flexNVM partition works.

It seems that th epartition command can not be executed if the memory is already partitioned.

The only way I found is to use Erase All Blocks command before to set a new partition.

Obviously this is not so useful, because of the Erase All Blocks delete my program code also.

What's the correct way to change a partition of a CPU?

ラベル(1)
1 返信

1,250件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

There is no workaround for the mass-erase. The partitioning is supposed to happen only once.

In application note AN4282 - Using the Kinetis Family Enhanced EEPROM functionality chapter 3.1 you will find the next:

Partition.png

Hope this is useful.

Regards!

Jorge Gonzalez

0 件の賞賛
返信