Kinetis Flash memory read error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis Flash memory read error

4,722 次查看
sandeepkamath
Contributor I

HI,

I have a problem with read operation from flash memory.

While testing of the code, we found a strange problem with flash memory.

For example: If the write operation (done using Kinetis Flash driver)is unsuccessful and during my next reboot if i try to read the specific location of the memory where it (got halt/ corrupted etc) was unsuccessful, i get a hard fault.

 I was expecting that kinetics controller will handle the data integrity automatically.

can you give me any suggestion on handling this issue. Is there any built in driver which will solve this reading issue( like detection of corrupted memory)

Thanks in advance

Sandeep

0 项奖励
回复
5 回复数

3,917 次查看
mjbcswitzerland
Specialist V

Hi

Hard Faults reading program Flash memory 

https://community.nxp.com/message/574401?commentID=574401#comment-574401 

And various others when a search for "hard fault Flash" is made.

Regards

Mark

0 项奖励
回复

3,917 次查看
sandeepkamath
Contributor I

Hi

Thanks for the response.

I thought we will be reading the garbage value instead of getting hard fault.

So If some thing goes wrong while writing, then it will go to hard fault while reading ??

0 项奖励
回复

3,917 次查看
mjbcswitzerland
Specialist V

Sandeep

It depends on the Kinetis part being used. Newer parts (like K64) will hard-fault if the Flash area is corrupted - older types may not. There is no official documentation about this behavior but can be observed with various parts.

Regards

Mark

0 项奖励
回复

3,917 次查看
sandeepkamath
Contributor I

Hi Hui_Ma, Hi Mark

Thanks for the response.

We are observing this hard fault in K24F series. Thanks for letting us know about this behavior. 

Regards,

Sandeep

0 项奖励
回复

3,917 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Embedded flash memory is grouped into blocks. Each block contains the circuitry required to read, erase, and program within that block. Most of the flash memory technologies have a limitation of not allowing read operations at the same time as an erase or program operation is occurring within the same block. Thus, erasing/programming a sector is not allowed if code execution (fetching instructions = reading) is taking place within the same block even if the read is in a different flash sector than the erase/program. This is called a Read While Write (RWW) violation and will result in a Read Collision error on Kinetis and other micro-controllers.

More detailed info, please check application note AN4695.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复