Kinetis Examples - broken Build - out of the Box USB Stack 3.2 and Codewarrior 10.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Examples - broken Build - out of the Box USB Stack 3.2 and Codewarrior 10.2

1,376 Views
eli_hughes
Contributor V

Hello:

 

I just downloaded the USB Stack 3.2.0. I imported 2 projects into Codewarrior 10.2:

Kinetis_MK20DX128VLH5_cdc and
Kinetis_MK40N512VMD100_cdc

 

Both of these projects have compile errors:

"The File "USB_BSP.h" cannot be opened"
"Undefined indentifier 'MCG_S_OSCINIT0_MASK'

 

I read through the documentation and there was no inidication that I had to modify these examples to get them to work.

 

Has anyone else seen this?

0 Kudos
Reply
2 Replies

1,052 Views
Spikey_Mikey
Contributor II

I had the same problem compiling under Windows 7.  I think it is a permission problem with copying the files over to the workspace.  I pulled up XP mode and installed CW 10.2 and USB Stack 3.2 and tried importing a CDC project and compiled it just now.  It looks like it works.

0 Kudos
Reply

1,052 Views
bigredhdl
Contributor I

I'm getting the same thing.

0 Kudos
Reply