Kinetis Device is locked

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis Device is locked

4,186 次查看
durgeshk
Contributor II

Hi,

I am using MKL16Z256VLH4 controller, when trying to download code ,getting message " Kinetis device is locked ! Do you want to unlock it ? Mass erase will be executed ! ". see below

Screenshot (22).png

 Clicking OK or Cancel displays message: " Cannot access memory".

Screenshot (23).png

I have tried it in keil with ULINK-ME 

Screenshot (25).png

how do i unlock please help.

标签 (1)
4 回复数

3,057 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Do you have a Segger J-Link tool on hand?

If yes, I would recommend to download and use Segger J-Link Commander tool to unlock KL16 chip.

pastedImage_1.png

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,057 次查看
durgeshk
Contributor II

Hi Hui_Ma

Thank you for reply

I don't have J-Link tool, I'm using Ulink2/ME..how to unlock with this tool

Regards 

Durgesh

0 项奖励
回复

3,057 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Durgesh,

Please check below link if that could help to fix the issue:

ULINK: UNLOCKING FREESCALE KINETIS MEMORY WITH ULINK 

Wish it help.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,057 次查看
andrewbarningha
Contributor III

Perfect - I wish all problems had answers like this.

0 项奖励
回复