Kinetis DMA sources/slot assignments

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis DMA sources/slot assignments

Jump to solution
2,934 Views
richyankee
Contributor II

For DMA - the DMAMUX  needs to have the peripheral slot (DMAMUX_CHCFGn) in the channel source of this register, Isee from a couple of examples on the forum that these are defined (in some include file), but I cannot find the file that contains these definitions.

 

Using IAR, K60 devkit (tower). The user guides and reference manuals say that the peripheral slots are defined in the 'device's Chip Configuration details'. Okay, I have the sub family ref manual, and the peripheral module quick ref.

 

I have the whole MQX developmentn tree and can't find the peripheral slots defined there (maybe I just don't know teh magic words to search for: like peripheral, slot, mux assignment etc.)

 

This is probably easy for somebody who has already set up a dma.

 

Thanks.

 

Rich

 

0 Kudos
Reply
1 Solution
1,815 Views
comsosysarch
Contributor III

https://community.freescale.com/thread/94844

 

K60 Sub-Family Reference Manual, Rev. 6, Nov 2011

pp 92-94

3.3.9.1 DMA MUX request sources

Table 3-24. DMA request sources - MUX 0

 

View solution in original post

0 Kudos
Reply
1 Reply
1,816 Views
comsosysarch
Contributor III

https://community.freescale.com/thread/94844

 

K60 Sub-Family Reference Manual, Rev. 6, Nov 2011

pp 92-94

3.3.9.1 DMA MUX request sources

Table 3-24. DMA request sources - MUX 0

 

0 Kudos
Reply