Kinetis + CodeWarrior JTAG TAP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis + CodeWarrior JTAG TAP?

3,357 Views
gloucks
Contributor III

Is there a TAP device available to allow CodeWarrior to attach to the JTAG on my (future) production Kinetis board (like with my 56k devices)?

 

And is there a device available that allows the flash to be programmed thru the ezPort?

 

0 Kudos
Reply
3 Replies

2,848 Views
gloucks
Contributor III

Let me rephrase the question:

 

1. What hardware/K60-feature do I need on my board to bring up a production K60 board?

 

2. What tool connects my production board to CodeWarrior?

 

3. What tool can I use to program the ezPort? Would it be the same tool as 2?

0 Kudos
Reply

2,848 Views
TravisHidlay
Contributor III

I have pretty much the same questions; in addition, for #2, what else is needed to allow debugging the code from CW on a production board?

0 Kudos
Reply

2,848 Views
pgo
Senior Contributor V

 

The kinetis device is supported by a few JTAG BDMs that support debugging and programming.  Search for the following:

Commercial:

Hobby/Open source

Any of these should work with the "standard" 10-pin or 20-pin JTAG interface.  You can look at the Freescale demo boards for example connector circuits.

 

Bye

0 Kudos
Reply