Kinetis Bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Bootloader

3,099 Views
Shawn_Lee
Contributor I

hello,

I download a file of following link

Kinetis Bootloader|Freescale

When I compile, the compiler result an error what it can't find bootloader_config.h

So where is bootloader_config.h?

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

2,539 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Shawn,

I think you are using Kinetis Bootloader with below link:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KBOOT

You could find the <bootloader_config.h> at below default path:

C:\Freescale\FSL_Kinetis_Bootloader_1_0_2\targets\k64f12\src


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,539 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Shawn,

Your link I can't open , is my mistaken ?

Alice

0 Kudos
Reply

2,539 Views
Shawn_Lee
Contributor I

Sorry Alice, I have fixed the link.

0 Kudos
Reply

2,539 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Shawn,

Have you refer to the "Gettin_Started_with_Freescael_KInetes_K64_Bootloader.pdf"  on "....FSL_Kinetis_Bootloader_1_0_2\FSL_Kinetis_Bootloader_1_0_2\doc"   ?

Hope it helps

ALice

0 Kudos
Reply