Kinetics selection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,237件の閲覧回数
d2014
Fresh Out Contributor

I am having trouble selecting the proper Kinetis MCU for evaluation for my new product. I have noticed that the SPI pins are the same as the UART pins. So I need the following connections: 1 or 2 SPI with 7 total CS pins, 2 RS485 UART, USB, DMA, 3.3V, 50+MHz, prefer no BGA package. Application is industrial control.

タグ(1)
0 件の賞賛
返信
1 解決策
2,119件の閲覧回数
mjbcswitzerland
Specialist V

David

I would start looking at the K20DX256x7 (as on the TWR-K20D72M)

- USB

- 2 SPIs

- 6 UARTs

There are a number of alternative pin mux options for these so you should have no problems finding the combination that you need

- 72MHz

- 100 pin LQFP

Then you could optimise on the package if needed (there are variations with less pins) and possibly on the peripherals (such as the K21 or K22) or choose parts with mort or less FLASH/RAM, max frequency or FPU.

Regards

Mark

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,119件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi David,

  Have you checked out the MCU solution advisor? For certain devices it'll even do the pin muxing solving for you http://freescale.transim.com/solutionadvisor/SolutionAdvisor.aspx?t=features

  Mark has good suggestions as well, those should fit your needs well.

-Anthony

2,120件の閲覧回数
mjbcswitzerland
Specialist V

David

I would start looking at the K20DX256x7 (as on the TWR-K20D72M)

- USB

- 2 SPIs

- 6 UARTs

There are a number of alternative pin mux options for these so you should have no problems finding the combination that you need

- 72MHz

- 100 pin LQFP

Then you could optimise on the package if needed (there are variations with less pins) and possibly on the peripherals (such as the K21 or K22) or choose parts with mort or less FLASH/RAM, max frequency or FPU.

Regards

Mark

0 件の賞賛
返信