Keil Simulate has error for MK22

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Keil Simulate has error for MK22

1,376 Views
chengdong
Contributor I

hi,

when I install the KSDK 1.3,   I open an example project use keil mdk.  after sucessfully build the project, but I can't use simulater to debug. 

pastedImage_1.png

I think maybe I use a wrong parameter for MK22FN512, I look for some manuals for MK22, but i can't 

find the right parameter.

pastedImage_5.png

so could you tell me the right parameter, or MK22 is not supported for simutaler?

thank you!

Tags (1)
0 Kudos
Reply
1 Reply

1,294 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi
You can have a look at "uVISION DEBUGGER: Simulation of Cortex-M Devices", the K22 is not on the list.
The 0x4005200E is the address of WDOG.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply