KW45 based BLE dongle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW45 based BLE dongle

Jump to solution
2,145 Views
tomaru
Contributor III

Dear Team,

I look over the NXP product lineup and say many MCU have a BLE dongle which best suits some application for Testing and development.

I want to know if any such device exists for KW45 MCU?
I am in real need for KW45 based dongle.

If it does not exist - 
1. Do we have any other dongle which I can use to receive data over BLE which I can program the same code made for KW45 MCU ?

2. I know point 1 is difficult, but if we can migrate code from KW45 to other MCU and do this?
Example - KW40 can use same code by migrating KW45 code and doing some changes.

If 2 is possible, can you provide MCU details and Migration guide if available?

BR,
Tomaru

USB-KW38 USB-KW41Z BLE-NFC KW45B41Z-EVK KW45 

Tomar Ankit
Labels (1)
0 Kudos
Reply
1 Solution
2,102 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @tomaru 

I am so sorry for the inconvenience because we do not have a USB-Dongle based on KW45 BLE chip.

1. Do we have any other dongle which I can use to receive data over BLE which I can program the same code made for KW45 MCU ?

==>Sorry, we do not have.

2. I know point 1 is difficult, but if we can migrate code from KW45 to other MCU and do this?

==>Sorry, I worry it is not possible. 

You might think about our other USB-Dongles such as USB-KW38, USB-KW40, USB-KW41.

I know it is not convenient for you, but currently, we do not have such kind of dongle for KW45 and also not possible to migrate code from KW45 to other USB-Dongles.

 

Best regards,

Christine.

View solution in original post

0 Kudos
Reply
2 Replies
2,103 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @tomaru 

I am so sorry for the inconvenience because we do not have a USB-Dongle based on KW45 BLE chip.

1. Do we have any other dongle which I can use to receive data over BLE which I can program the same code made for KW45 MCU ?

==>Sorry, we do not have.

2. I know point 1 is difficult, but if we can migrate code from KW45 to other MCU and do this?

==>Sorry, I worry it is not possible. 

You might think about our other USB-Dongles such as USB-KW38, USB-KW40, USB-KW41.

I know it is not convenient for you, but currently, we do not have such kind of dongle for KW45 and also not possible to migrate code from KW45 to other USB-Dongles.

 

Best regards,

Christine.

0 Kudos
Reply
2,032 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @tomaru 

Anything else I can do for you on this case?

If no other concerns, would you mind to mark my answer as a solution for this case so that we can close this thread?

Please feel free to create new case to us if you meet any other issue during using our products.

 

Best regards,

Christine.

0 Kudos
Reply