KW36A BUCK AUTOSTART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW36A BUCK AUTOSTART

1,082件の閲覧回数
kiransajeev
Contributor I

Hello,

I want to use KW36A chip in buck auto start mode. I have the VDCDCIN and DCDC-CFG and PSWITCH wired together.

Is it all thats required to power up the MCU?

I have not connected the 1P8OUT back to the VDD0 and VDD1 pins. Is there any issues with not doing that?

What are the implications if VDD0 and 1 are in the NC state?

I have connected VDDA, VREFH to 1P8OUT. Will that suffice?

Regards,

Kiran

0 件の賞賛
返信
1 返信

1,043件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

Yes, you need the VDD_0 and the VDD_1 connection. For further details, you can seen in our FRDM-KW36 Minimum BoM Development BoardUser’s Guide , in chapter 3 the connections needed for the requested configuration.

pastedImage_6.png 

Regards,
Estephania

0 件の賞賛
返信