KW36 power mode for advertising

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW36 power mode for advertising

1,530件の閲覧回数
bob_zhang
Contributor I

If let KW36 work in advertising mode(interval is 100ms),all peripherals can be off. Which power mode should I select for best power consumption performance?

ラベル(1)
0 件の賞賛
返信
1 返信

1,445件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Bob, I hope you're doing well!

 

During BLE Advertising, the device cannot be in sleep mode, as the transceiver is turned off during any of the low-power modes. Depending on the low-power mode, transceiver digital logic is either power-gated, or has its state retained.

 

For more information about low-power modes for the KW36 and implementation in BLE applications, could you please take a look at the Kinetis MKW36 Power Consumption Analysis document?

 

As for which specific power mode should be implemented for the time when the MCU is not advertising, it will vary depending on the capabilities which you wish to retain during this time, as well as the wake-up sources.

 

Chapter 8 of the MKW36/35/34 Reference Manual contains Table 8-2, which describes each of the modules' operation conditions for every power mode.

 

Please let me know if you need any more information.

 

Best regards,

Sebastian

0 件の賞賛
返信