KW36 Erase failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW36 Erase failure

1,859 Views
nsuresh2
Contributor III

Hi XingChang,

 

I am working on KW36 micro and I am using J Link Plus debugger to flash the firmware using J Link commander v6.44.

For one of our application, I need to do read/write/erase part of the internal flash. Which caused the device unusable. Tried to do unlock as per the instructions from JLink unlock is successful but fails in erasing the flash.

 

Please find the below and attached logs from J Link commander:

 

J-Link>connect

Please specify device/core. <Default>: MKW36Z512XXX4

Type '?' for selection dialog

Device>

Please specify the target interface:

  1. J) JTAG (Default)
  2. S) SWD
  3. T) cJTAG

TIF>s

Specify the target interface speed [kHz]. <Default>: 4000 kHz

Speed>

Device "MKW36Z512XXX4" selected.

 

 

Connecting to target via SWD

InitTarget()

Readout protection is set and mass erase is disabled. J-Link cannot unprotect th

e device.

Found SW-DP with ID 0x0BC11477

Scanning AP map to find all available APs

AP[2]: Stopped AP scan as end of AP map has been reached

AP[0]: AHB-AP (IDR: 0x04770031)

AP[1]: JTAG-AP (IDR: 0x001C0020)

Iterating through AP map to find AHB-AP to use

AP[0]: Core found

AP[0]: AHB-AP ROM base: 0xF0002000

CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)

Found Cortex-M0 r0p1, Little endian.

FPUnit: 2 code (BP) slots and 0 literal slots

CoreSight components:

ROMTbl[0] @ F0002000

ROMTbl[0][0]: F0000000, CID: B105900D, PID: 001BB932 MTB-M0+

ROMTbl[0][1]: F0001000, CID: B105900D, PID: 0008E000 MTBDWT

ROMTbl[0][2]: E00FF000, CID: B105100D, PID: 000BB4C0 ROM Table

ROMTbl[1] @ E00FF000

ROMTbl[1][0]: E000E000, CID: B105E00D, PID: 000BB008 SCS

ROMTbl[1][1]: E0001000, CID: B105E00D, PID: 000BB00A DWT

ROMTbl[1][2]: E0002000, CID: B105E00D, PID: 000BB00B FPB

Cortex-M0 identified.

J-Link>unlock Kinetis

Found SWD-DP with ID 0x0BC11477

Unlocking device...O.K.

J-Link>erase

Erasing device...

 

****** Error: Failed to erase sectors 0 @ address 0x00000000 (Unspecified error

#2)

J-Link: Flash download: Total time needed: 0.066s (Prepare: 0.055s, Compare: 0.0

00s, Erase: 0.005s, Program: 0.000s, Verify: 0.000s, Restore: 0.005s)

ERROR: Erase returned with error code -5.

J-Link>

Regards,
Naven Suresh

0 Kudos
Reply
1 Reply

1,747 Views
xing_chang
NXP Employee
NXP Employee

Hi [email protected]‌,

You can use J-Flash Lite to erase chip.

pastedImage_1.png

0 Kudos
Reply