KW21Z to replace KW41Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW21Z to replace KW41Z

Jump to solution
2,332 Views
paralax
Contributor I

Hi.

I need to make a production, and I currently use a KW41Z. Of course, it's near impossible to find any stock, and the lead time is now 52 weeks.

I only use the SMAC 802.15.4 stack, so it seems I can use the KW21Z as a drop in replacement. Can you confirm that it is a direct replacement?

Should I change the init vector (or other stuff?), and is the SMAC stack still compatible (I just modified it a bit to not use the common library and call directly my freertos routine, but the core of the library has not changed)

 

Regards,

 

Matthieu 

Labels (1)
0 Kudos
Reply
1 Solution
2,308 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Matthieu,

 

Hope you are doing well. Yes, you can use the KW21Z if you are interested in 802.15.4.

Just be sure to buy the same Package, Flash and SRAM version.

Ricardo_Zamora_1-1619808560472.pngRicardo_Zamora_1-1619808560472.png

 

Best Regards,

Ricardo

View solution in original post

1 Reply
2,309 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Matthieu,

 

Hope you are doing well. Yes, you can use the KW21Z if you are interested in 802.15.4.

Just be sure to buy the same Package, Flash and SRAM version.

Ricardo_Zamora_1-1619808560472.pngRicardo_Zamora_1-1619808560472.png

 

Best Regards,

Ricardo